[WATCHLIVE]NOW!] Centennial vs Chaparral High school football player dies after suffering head injury during game. High School football Quarterbacke. 'Will Never Be Forgotten' A local community is mourning Caden Tellier, generosity and love Caden Tellier, the quarterback for Morgan Academy, died Saturday home opener night, his family confirmed on social media. The ASWA prep committee's primary responsibilities include conducting regular top-10 rankings of a variety of high school sports, and select all-state teams in those sports as well. The committee will determine the winner of a variety of annual awards including the annual Mr. Football winner, and the Jimmy Smothers Courage Award. After three weeks of the season, only two No. 1 ranked teams in the Alabama Sports Writers Association prep football rankings received all 18 first-place votes. Reigning 7A champ Central-Phenix City continues to be a unanimous choice in its classification, while Jackson also received all the No. 1 votes in Class 4A. Vinson had seven receptions with 143 yards and one touchdown in their 12-10 win over Houston Academy. Vinson is listed as a three star and holds offers from Arkansas, Tennessee, Vanderbilt, and other schools as well according to 247Sports. This time, all being well, United will appoint a manager with a record of success at home and in Europe, a manager whose achievements are in the present and not the past, a manager who has both nothing and something to prove. You'd think that would be the baseline for anybody coming into the job, and yet the last time they did that it was 1986. This is not to compare Ten Hag and Alex Ferguson; that would obviously be unhelpful. But it's about time a United board took the managerial appointment seriously. You'd expect them to be Aston Villa, especially if Jack Grealish is still missing. But then they have the second leg against Real Madrid. Championship fixtures | table | highlightsGet Sky SportsMid-table Stoke had ended a winless run of eight league games with successive home wins over Millwall and Sheffield United. “We probably have to learn how to be more consistent in a long season. To be in the top four, it has to be on a consistent basis. We’ve got Burnley in midweek – they’re fighting for their lives so we know it’ll be a tough one.” Talking of Hull, their standout festive moment - and a unique episode in Premier League history - came at Etihad Stadium in 2008 when boss Phil Brown gave his side a half-time dressing down on the pitch. The Bulldogs opened up the season with an impressive win and performance from Thornton. The signal caller finished completing 8-of-9 passes for 148 yards and three touchdowns.